cancel
Showing results for 
Search instead for 
Did you mean: 

How to set the parameters of the LTDC controller?

GMeur
Senior II

Hola,

I need your help in order to configure the LTDC controller of my project because I've a very limited knowledge of LCD screens. After having read this tutorial, everything appeared clear and I thought it would be straightforward to configure my file. Little did I know that the documentation of my screen would use a rather different terminology and that I can't translate between the twos. Plus, it seems that some parameters are missing from the doc… The datasheet of the screen is attached to this message.

All I need to configure to get it working are these few lines I think :

hltdc.Init.HorizontalSync = 40;
    hltdc.Init.VerticalSync = 20;
    hltdc.Init.AccumulatedHBP = 46; //Acculumutaled Horizontal Back Porsh
    hltdc.Init.AccumulatedVBP = 23; //Accumulated Vertical Back Porsh
    hltdc.Init.AccumulatedActiveW = 846;
    hltdc.Init.AccumulatedActiveH = 503;
    hltdc.Init.TotalWidth = 886;
    hltdc.Init.TotalHeigh = 523 ;

(located in HW_Init.cpp)

A huge thanks in advance.

0 REPLIES 0