2025-08-03 11:10 PM
Hello All,
I have created one project which is working on STM32H747i- Eval board with 800 x 480 resolution, now the project has to be migrated to 1024 x 600 resolution for larger display.
I have migrated the backend code but now the Screen resolution is still 800 x 480 and the widgets are aligned to work with it.
Now how shall I configure the project to 1024 x 600, I mean is there any to do it instead of manually adjusting the screens and widgets ?
If there is any effective and better solution kindly do let me know ?
Regards,
Shiv