cancel
Showing results for 
Search instead for 
Did you mean: 

how to get the 7" LTDC to work with stm32h743ii on a waveshare board?

WBeck.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4

Get the screen geometry and timing correct.

The timing is frequently dependent on the resolution, not the physical size.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
WBeck.1
Associate

Yes I understand that, thank you for answering. I am trying to start a project in touchGFX and I can not find a demo or example for a STM32H743II.

ktrofimo
Senior III

Question is - what display model you are using and what touch IC it has. You will need datasheets for both of them.

Display datasheet will give you timing information for LTDC (screen viewable pixels, pixelclock, FP, BP).

For Touch IC you will need to use either existing driver (if you are lucky) or write your own having some driver as an example and implement data communication (usually over I2C or SPI) according manufacturer datasheet. Please note that some touch ICs have only linux open source driver and then you will need to port it to STM.

KMacf.1
Associate II

Actually, I don't think you need front & back porch lengths in terms of number of pixel clocks any more - LCD seem to have got smarter & are more tolerant of the Hsync & Vsync pulse FP & BP lengths. As long as there's an Hsync & a Vsync, that's sufficient.