2024-10-25 02:52 AM
I developed firmware with CUBE IDE and then set up the 2.4" TFT LCD screen with buttons, etc., using TOUCH GFX DESIGNER. How do I import what I developed in TOUCH GFX into CUBE IDE?
Solved! Go to Solution.
2024-10-25 04:23 AM
Hello @Emanuele78 ,
Once you have created you desired GUI, simply click on "Generate code" on the bottom right corner:
Then you can simply open the folder of your project on the bottom left:
Finally, open your STM32CubeIDE project in the STM32CubeIDE project.
Also, you can look at this video : How to TouchGFX: Creating my first GUI with TouchGFX Designer for STM32 GUI applications
Hope this help! :smiling_face_with_smiling_eyes:
If this answers your question, I invite you to select this comment as "best answer".
Regards,
2024-10-25 04:23 AM
Hello @Emanuele78 ,
Once you have created you desired GUI, simply click on "Generate code" on the bottom right corner:
Then you can simply open the folder of your project on the bottom left:
Finally, open your STM32CubeIDE project in the STM32CubeIDE project.
Also, you can look at this video : How to TouchGFX: Creating my first GUI with TouchGFX Designer for STM32 GUI applications
Hope this help! :smiling_face_with_smiling_eyes:
If this answers your question, I invite you to select this comment as "best answer".
Regards,
2024-10-25 06:27 AM - edited 2024-10-25 08:22 AM
Thank you, I managed to import the file created in TouchGFX into the IDE. Now, for the next step, how do I integrate it into the IDE firmware I've already written? How should I proceed? Which folders do I need to copy from the TouchGFX file to the IDE?
In the attached screenshot, you can see the two projects open. Thanks again.
2024-10-25 03:09 PM
To many files. folders and adding paths to deal with. You're better off copying your files from the other project into the TouchGFX project.