cancel
Showing results for 
Search instead for 
Did you mean: 

How can I use one of the 8BPP format (e.g. ARGB2222)

egoltzman
Senior

Hi,

I want to try to use 8BPP in one of the project I'm working on.

I set the LTDC to work in 8BPP and I tried to define a designer project that is configure with 8bpp.

When I try to change the config I get error messages that I can not use this format

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Martin KJELDSEN
Chief III

Hi Eyal,

ARGB2222 (8-bit) is supported in TouchGFX 4.11+. Even though the release is completed and we have the binary, it's not officially released because of internal release dependencies. 4.12 will be out as soon as CubeMX 4.4.0 is released.

/Martin