2020-02-25 12:24 AM
Hi,
I want to use an image stored in µSD card.
I found the following exemple : STM32Cube_FW_F7_V1.15.0\Projects\STM32746G-Discovery\Applications\Display\LTDC_PicturesFromSDCard
But it is a still image.
What I want to do :
Create the design with TouchGFX. But the size of all images is larger than the size of flash (1 Mo). Can I use an SD card to "replace" objects on the design ?
2020-02-25 12:58 AM
Hi @MMerc.1,
To do that with TouchGFX you have to use something we call Bitmap Caching. Let me start you off by providing this link - Same would apply for an SD card.
You will need some form of cache in SDRAM and then you usually cache the images you need for a particular screen. But, it impacts render times, so you could cache a lot of images during startup if you have the memory, for instance. There are a variety of options depending on performance requirements and available hardware.
/Martin
2020-02-25 1:16 AM
Hi Martin,
Thank you for your advice.
I will come back to you if I have questions.
2020-02-25 2:12 AM
From what I understand, I have to add the following code in the initialization of TouchGFX :
// Place cache start address in somewhere SDRAM
uint16_t* cacheStartAddr = (uint16_t*)SDRAM_CACHE_START;
uint32_t cacheSize = 0x300000; //3 MB, as example
HAL& hal = touchgfx_generic_init<STM32F4HAL>(dma, display, tc, DISPLAY_WIDTH, DISPLAY_HEIGHT, cacheStartAddr, cacheSize);I have the following code :
void touchgfx_init()
{
Bitmap::registerBitmapDatabase(BitmapDatabase::getInstance(), BitmapDatabase::getInstanceSize());
TypedText::registerTexts(&texts);
Texts::setLanguage(0);
FontManager::setFontProvider(&fontProvider);
FrontendHeap& heap = FrontendHeap::getInstance();
(void)heap; // we need to obtain the reference above to initialize the frontend heap.
hal.initialize();
}Should I add the previous code after hal.initialize() ?
After that, it talk about SDRAM. Should I add this from CubeMX (Middleware -> FATFS -> External SDRAM) ?
How can I change the address of ExtFlashSection ?
How can I place the entire contents of ExtFlashSection in a single binary file ?
Concerning the platform specific driver, when it talks about "subclass", is it an heritage ?
It is very well explained but it lacks exemples like "Getting started"...
2020-03-02 6:41 AM
UP please
2020-03-02 9:04 AM
>>How can I change the address of ExtFlashSection ? How can I place the entire contents of ExtFlashSection in a single binary file ?
Presumably by modifying the linker script or scatter file. I'd probably figure out a way of letting the linker do the bulk of the work, pretend that SDRAM content, or a portion at least, behaves like FLASH, and then extract the section from the .ELF/.AXF file to file(s) I can put on SD Card, and then load them into SDRAM early in main(), or prior.
2020-03-03 12:40 AM
Hi Clive,
Thank you.
How can I do this ?
2020-03-03 6:05 AM
You actually don't have to call touchgfx_generic_init() if you're using the TouchGFX Generator. e.g. But there's no support for cache currently in the Generator. We took it out because it was a bit too application specific.
The below is what you're getting from the Generator in TouchGFXConfiguration.cpp. This is a generated file that will get overwritten if you re-generate.
...
static TouchGFXHAL hal(dma, display, tc, 480, 272);
void touchgfx_init()
{
Bitmap::registerBitmapDatabase(BitmapDatabase::getInstance(), BitmapDatabase::getInstanceSize());
TypedText::registerTexts(&texts);
Texts::setLanguage(0);
FontManager::setFontProvider(&fontProvider);
FrontendHeap& heap = FrontendHeap::getInstance();
(void)heap; // we need to obtain the reference above to initialize the frontend heap.
hal.initialize();
}So, what you have to do here is to add the code inside the Generated TouchGFX HAL class (one big user code section where you can write stuff). It implements HAL::initialize() and calls its super class version of the same, so put the re-configuration of BitmapDatabase here - something like:
void TouchGFXHAL::initialize()
{
// Calling parent implementation of initialize().
//
// To overwrite the generated implementation, omit call to parent function
// and implemented needed functionality here.
// Please note, HAL::initialize() must be called to initialize the framework.
TouchGFXGeneratedHAL::initialize();
Bitmap::registerBitmapDatabase(BitmapDatabase::getInstance(),
BitmapDatabase::getInstanceSize(),
bitmapCache,
bitmapCacheSize,
numberOfDynamicBitmaps);
}
2020-03-03 6:34 AM
Hi Martin,
Thank you.
The following variables correspond to :
2020-06-01 5:01 AM
You're right, it's really the introductory example that's needed for newbies.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.