2020-01-13 6:37 AM
I use the demo board STM32H750B-DK, the CubeIDE 1.2, and TouchGFX 4.13.
I followed the following guides and set the pins as default:
https://touchgfx.zendesk.com/hc/en-us/articles/360011039799-Installing-TouchGFX
https://touchgfx.zendesk.com/hc/en-us/articles/360010921760-TouchGFX-HAL-Development
First there was a build error because of flash overflow. To solve this I edited STM32H750XBHx_FLASH.Id by using the settings of a working TouchGFX (v4.10) project.
/* Memories definition */
MEMORY
{
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
/* FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 128K*/
FLASH (rx) : ORIGIN = 0x90000000, LENGTH = 2048K
ASSETS_FLASH (r) : ORIGIN = 0x90200000, LENGTH = 126M
SDRAM (rw) : ORIGIN = 0xD0000000, LENGTH = 8M
}
ExtFlashSection :
{
*(ExtFlashSection ExtFlashSection.*)
*(TextFlashSection TextFlashSection.*)
*(FontFlashSection FontFlashSection.*)
*(.gnu.linkonce.r.*)
. = ALIGN(0x4);
} >ASSETS_FLASH
Now I can build without any error.
Then I flashed the board with the CubeProgrammer v2.1.0.
The gui should be a textured background with a labled button. However the display is just white.
Has anyone any ideas about this?
Thank you.
2020-01-15 12:22 AM
Is the application running?
/Martin
2020-01-20 5:29 AM
Hi Martin
Yes, it is running. I toggle an LED in the same task in which TouchGFXProcess() is called. I also tried to use another task for the LED. The LED toggles fine but the display stays white.
Other things I tried are:
I use the external SDRAM so that there is enough memory for the framebuffer. That only works with the ExtMem_Boot of a TouchGFX-Designer project, not with the bootloader of the firmware package.
Increase the stack and heap.
Store TouchGFX-data into the external flash 0x90200000.
Deactivate Ethernet in CubeMX for the application.
Deactivate QSPI in CubeMX for the application because it has already be done in the bootloader.