cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I can't open my TouchGFX project. The message that appears is the following "reference to an object not set on an object instance" Can you help me? Regards, Luca

LucaCMA
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
16 REPLIES 16
Martin KJELDSEN
Chief III

I need way more information than that :) Version? What've you tried? Share your project?

Thanks

LucaCMA
Associate II

Hi Martin,

TouchGFX Designer Version 4.12.3

SLA0044 Rev5/February 2018

LucaCMA
Associate II

Sorry....correct project

TouchGFX Designer Version 4.12.3

SLA0044 Rev5/February 2018

LucaCMA
Associate II

Hi,

do you have an idea for this problem?

Regards,

Martin KJELDSEN
Chief III

Hi Luca,

4.13.0 will be out this week so let's see if that solves things for you. I'm pretty sure we've fixed an issue similar to what you're seeing here.

/Martin

Sjohn.1
Associate

Hi, I have simillar issue with Cubemx 5.5.0 and TouchGFX 4.13.0

error msg : "Object reference not set to an instance of an object."

Martin KJELDSEN
Chief III

Are you trying to open up a possibly broken project in 4.13.0 ? Please show me a log for 4.13.0.

Kelsey
Associate

Is there a solution for this? I am having the same problem in my project. I was trying to upgrade my project from 4.12.3 to 4.13 and ran into this error. I can message the zip of my project if necessary.

LucaCMA
Associate II

I still have the same problem with 4.13