Hardware mistake and LTDC remapping solution wanted!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-08 10:56 AM
Hello everyone, I have a big problem with the hardware. I designed the hardware before dealing with the Cubemx. Starting from a circuit that worked, I mistakenly thought that giving the system RGB666 from RGB888 meant giving bits 0 to 6 R0...R6, G0..G6, B0..B6. I then connected the two bits of the display R0, R1, G0, G1, B0 B1 to ground, as shown in the figure. But I have the problem that everything is wrong.Is it possible to remap LTDC so I can see everything properly?
Thanks for your help.
Solved! Go to Solution.
- Labels:
-
STM32CubeMX
-
TouchGFX Designer
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-10 2:12 AM
Simply in MX wizard change ltdc layer 0 to L8 and same touchgfx buff to L8 and regenerate target.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-09 3:03 AM
Ok, I understand that this is not possible to do on the LTDC, I just read the datasheet, but it is instead possible to manipulate the color file on touchgfx, but I would have to override the setBitmap(const Bitmap& bmp) function similar to readBMP24File and shifting the pixels, it would Is a similar solution possible or not? premise, I set the HW as RGB888 and it works and then deinitialized the x6 and x7 pins of the RGB, and everything goes, now the color needs to be shifted downwards by two bits per color.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-09 8:48 AM
Ok, update: one part of problem solved changing file color.hpp, now the hard part is intercept ware the bitmap for widget is loaded and shift rgb, there is someone can help? can't find this in code. I can be very grateful for this, I have a demo and can't change hardware in this moment...
thanks.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-09 10:23 AM
LTDC is hw based transfer , you cant manipulate it, but you can change framebuffer data before LTDC use it.
Issue is speed and size of lcd. For example 320x240 you can simple change data in buffer, but for big displays MCU dont have power todo.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-09 10:50 AM
Hi MM..1, thanks for your answer. I 'm using H7, I can try to do it, ware is the specified point for buffer transfer whith touchgfx?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-09 11:28 PM
You have maybe next one choice, use L8 LTDC indexed mode 256 pallete system and modify generated array.
But here your design is limited to 256 colors.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-10 1:21 AM
Thanks for the suggestion, I wanted to modify the direct reading of the bitmaps from the external flash at loading, this would have made the computational cost minimal. I've already done this for colors where the change was quick. But I searched for hours for the link between the widgets and the load and I think it's closed in drawPartialBitmap(xx..), wouldn't there be a way to overwrite the function? regarding the tip with L8, is there an example of how to create the setting? Thank you.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-10 2:12 AM
Simply in MX wizard change ltdc layer 0 to L8 and same touchgfx buff to L8 and regenerate target.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-10 4:35 AM
MM..1, YOU SAVED ME! how this mechanism work? different bit/byte distribution? I'm a newbie on interfaces, I'm 12 years old on power systems... very distant from this field. Really thanks!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-10 5:22 AM
But now I have this proble, this is for L8? I don't understand...