cancel
Showing results for 
Search instead for 
Did you mean: 

Get an example TouchGFX

AD�?b
Senior

I wanted to use the example "Method 1 - From GUI task" TouchGFX. I downloaded PollDemoHwInt 4.9.3.zip. Unpacked. Can't open STM32CubeIDE 1.1.0?

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Martin KJELDSEN
Chief III

The example is based on 4.9.3 and was written before CubeIDE came out, i think. I'm guessing the reason you can't open it is because there's no cube ide project.

Please enlighten me if i'm wrong.

/Martin

This is. Can this be remedied?

Unfortunately not. At least not by us, right now. Which board are you going to try this on? And what are you trying to accomplish? I may be able to guide you in the right direction - E.g. the new v3 Application templates already come with .ioc files that you can open and configure additionally through CubeMX and generate a CubeIDE project. Then make your modifications for hardware integration with touchgfx according to the example you've just downloaded for inspiration,

/Martin

I came back to STM32CubeIDE 1.1.0. I am happy with that, therefore I will not return to version 1.2.0. I work on STM32F746G-DISCO.