2020-09-03 02:06 AM
Hi,
I'm trying to fade a group of images that are superposed, grouped in a container, but I have issues.
I tried using setAlpha for each component of the container, but then we see the images under that are part of this container.
I want the group of image to behave as one.
Then I tried to use the cacheable container, but when changing the alpha, the part that was transparent is now fading out, and we see the limit of the container :
Any idea how we can achieve what we want ? A nice fade in/out of multiple images as it was one image, keeping the transparency around ?
Thanks
2020-09-03 06:57 AM
Hi,
What do you mean by we see the images under that are part of this container? I dont understand from the photo what exactly you are looking for (how many objects are there, which one do you want to keep, ...). For example the power logo that is cut in half, cant you make the box behind a bit larger to prevent the cut? Or try to have the alpha of the power button a bit higher than the rest/reduce it at a lower pace.
For the cachebale container option, could you put a box of the same color as the background in the container under that you do not fade out?
Maybe add some images of the widgets used in Designer or some code.
/Romain
2020-09-03 10:29 AM
Thanks for the response, here's more information :
I hope my answer help you to understand my problem. Let me know if you need anything else.
Thanks
2020-09-08 02:34 AM
@Romain DIELEMAN Is the information is good ? Anyway to achieve what we want ?
Thanks
2020-09-14 02:46 AM
Is there anyone that can help ?
Thanks