2024-01-15 5:41 AM
I am trying to flash the STM32H753I-EVAL-2 board with a .hex file generated from STM cube IDE version 1.14.0.
The code is build without error, but while loading it using the STMCube Programmer, I am getting the following errors:
Error: Failed to download Segment [1]
These are the options that I have selected while starting the programming :
External Loader selected: M29W128GL_STM32H743I_EVAL
KIndly help.
2024-08-26 3:52 AM - edited 2024-08-28 11:45 PM
2025-10-28 7:33 AM
it depend on the file size