2022-11-04 6:29 AM
I'm using a STM32H743.
I used STM32CubeMx to configure the DCMI. It uses DMA to transfer to memory.
When calling HAL_DCMI_Start_DMA(), the DCMI_DMAError() function is called.
I found out that there is a transfer error. And according the documentation a bus error is the reason.
But the CFSR register of the MCU is zero, indicating no bus error.
What could be wrong?
Things I did:
Any idea why I can get this transfer error?
Solved! Go to Solution.
2022-11-06 3:22 AM
I found the problem! It is a bug of STM32CubeMx.
STM32CubeMx generates this code to initalize all peripherals:
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DCMI_Init();
MX_I2C1_Init();
MX_I2C2_Init();
MX_UART5_Init();
MX_USART1_UART_Init();
MX_DMA_Init();
MX_USB_DEVICE_Init();
The problem is that MX_DCMI_Init() initializes the DMA. But the DMA clock is not enabled yet! It is enabled by MX_DMA_Init().
I did not want to change the initialization order, so I enabled the DMA clock just before all the inits:
/* USER CODE BEGIN SysInit */
__HAL_RCC_DMA2_CLK_ENABLE();
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DCMI_Init();
MX_I2C1_Init();
MX_I2C2_Init();
MX_UART5_Init();
MX_USART1_UART_Init();
MX_DMA_Init();
MX_USB_DEVICE_Init();
And now it works!
2022-11-04 6:37 AM
>>But the CFSR register of the MCU is zero, indicating no bus error.
The MCU doesn't do the DMA, or have visibility, as to what the DMA Controller is doing / using.
Look at the Bus Matrix, and how that relates to the DMA Unit, and the Memory you're acting on.
Some memories are not visible / usable. Be sure of where your buffer is situated.
Check alignment.
2022-11-04 6:42 AM
Thx Tesla DeLoran
I'm using SRAM1 which should be accesable by the DMA. It starts at 0x30000000.
You say 'Look at the Bus Matrix': Do you mean to find out what the bus error is? Or do you mean that I have to program the Bus Matrix? (I assumed STM32CubeMx does that).
2022-11-06 3:22 AM
I found the problem! It is a bug of STM32CubeMx.
STM32CubeMx generates this code to initalize all peripherals:
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DCMI_Init();
MX_I2C1_Init();
MX_I2C2_Init();
MX_UART5_Init();
MX_USART1_UART_Init();
MX_DMA_Init();
MX_USB_DEVICE_Init();
The problem is that MX_DCMI_Init() initializes the DMA. But the DMA clock is not enabled yet! It is enabled by MX_DMA_Init().
I did not want to change the initialization order, so I enabled the DMA clock just before all the inits:
/* USER CODE BEGIN SysInit */
__HAL_RCC_DMA2_CLK_ENABLE();
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DCMI_Init();
MX_I2C1_Init();
MX_I2C2_Init();
MX_UART5_Init();
MX_USART1_UART_Init();
MX_DMA_Init();
MX_USB_DEVICE_Init();
And now it works!