cancel
Showing results for 
Search instead for 
Did you mean: 

DCMI with DMA interface to AXI_SRAM results in TRANSFER ERROR

DLane.1
Associate II

Hello

My setup contains an STM32H743 with a camera attached via DCMI interface.

I am trying to acquire single snapshot, but unfortunately experiencing errors.

I declared the following variable on my SRAM

#define BUFF_SIZE (160*120)
ALIGN_32BYTES(uint8_t frame_buff[BUFF_SIZE]);

the variable is allocated in the AXI_SRAM region (0x240....)

i also defined the MPU

  MPU_InitStruct.Enable = MPU_REGION_ENABLE;
  MPU_InitStruct.Number = MPU_REGION_NUMBER0;
  MPU_InitStruct.BaseAddress = D1_AXISRAM_BASE; // (0x24000000)
  MPU_InitStruct.Size = MPU_REGION_SIZE_512KB;
  MPU_InitStruct.SubRegionDisable = 0x0;
  MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
  MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
  MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
  MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
  MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE;
  MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;

and the DCMI's DMA intialized with

    /* DCMI Init */
    hdma_dcmi.Instance = DMA2_Stream1;
    hdma_dcmi.Init.Request = DMA_REQUEST_DCMI;
    hdma_dcmi.Init.Direction = DMA_PERIPH_TO_MEMORY;
    hdma_dcmi.Init.PeriphInc = DMA_PINC_DISABLE;
    hdma_dcmi.Init.MemInc = DMA_MINC_ENABLE;
    hdma_dcmi.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
    hdma_dcmi.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
    hdma_dcmi.Init.Mode = DMA_NORMAL;
    hdma_dcmi.Init.Priority = DMA_PRIORITY_HIGH;
    hdma_dcmi.Init.FIFOMode = DMA_FIFOMODE_ENABLE;
    hdma_dcmi.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;
    hdma_dcmi.Init.MemBurst = DMA_MBURST_INC4;
    hdma_dcmi.Init.PeriphBurst = DMA_PBURST_SINGLE;
    if (HAL_DMA_Init(&hdma_dcmi) != HAL_OK)
    {
      Error_Handler();
    }
 
    __HAL_LINKDMA(dcmiHandle,DMA_Handle,hdma_dcmi);
 
    /* DCMI interrupt Init */
    HAL_NVIC_SetPriority(DCMI_IRQn, 15, 0);
    HAL_NVIC_EnableIRQ(DCMI_IRQn);

then, starting the function

HAL_DCMI_Start_DMA(&hdcmi, DCMI_MODE_SNAPSHOT, (uint32_t)frame_buff, BUFF_SIZE);

I found out that my `frame_buff` is empty, and after debugging a while, found out that I keep getting a DMA IRQ which results with the error code

HAL_DMA_ERROR_TE

Please, help me find out the reason for the problem with the data transfer.

Sincerely

Dan

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
waclawek.jan
Super User

DMA2_S1CR is suspiciously set to byte transfer on both ports. You did not show us the FIFO control register for stream 1.

Can't this be consequence of the infamous "DMA needs to be enabled first" bug of the older CubeMX versions?

JW

View solution in original post

5 REPLIES 5
berendi
Principal

Please post the contents of the DMA, DMAMUX and DCMI registers before and after starting DMA.

Hello

Thanks for your response. I am attaching following register values (also via zipped folder).

My compiler allocated the `frame_buff` at `0x240222c0`, which is observed also in the DMA registers.

Please notice the register values -

before request:

0693W000001cIXDQA2.jpg

0693W000001cIXXQA2.jpg

0693W000001cIXcQAM.jpg

after request:

0693W000001cIXhQAM.jpg

0693W000001cIXmQAM.jpg

snapshot while in DMAError:

0693W000001cIXrQAM.jpg

0693W000001cIY1QAM.jpg

I noticed I get the `HAL_DCMI_VsyncEventCallback` + `HAL_DCMI_LineEventCallback` + `DCMI_IRQHandler` irq's but still, no data appending to the `frame_buff`.

Any idea what can result the problem?

Sincerely

Dan

qbaj
Associate II

Hi,

1)

did you try change destination for HAL_DCMI_Start_DMA?

I have problem with AXI_SRAM and SDRAM, but RAM1/2/3 works for me.

ALIGN_32BYTES(uint8_t buffer1[BUFFER_SIZE]) __attribute__((section(".RAM_D1"))); /*AXI_SRAM*/
ALIGN_32BYTES(uint8_t buffer2[BUFFER_SIZE]) __attribute__((section(".RAM_D2"))); /*SRAM1, SRAM2, SRAM3*/

2)

what size of image do you want download and which format?

#define BUFF_SIZE (160*120)

3)

do you have correct configuration for DCMI? PCK/VS/HS Polarity?

waclawek.jan
Super User

DMA2_S1CR is suspiciously set to byte transfer on both ports. You did not show us the FIFO control register for stream 1.

Can't this be consequence of the infamous "DMA needs to be enabled first" bug of the older CubeMX versions?

JW

DLane.1
Associate II

Initiating the DMA before the DCMI (initialization sequence) solved the issue.

Thanks