2025-11-26 12:15 AM
Hi,
using TouchGFX, I get the following error when I run the code.
How can I fix this?
Thanks
***************************************************************
Compiling simulator/main.cpp
Compiling touchgfx/framework/source/platform/driver/touch/SDL2TouchController.cpp
Linking build/bin/simulator.exe
m.AllocationBase 0x0, m.BaseAddress 0x60EA0000, m.RegionSize 0x370000, m.State 0x10000
C:\Programmi2\TouchGFX\4.26.0\env\MinGW\msys\1.0\bin\rm.exe: *** Couldn't reserve space for cygwin's heap (0x60EA0000 <0x1A90000>) in child, Win32 error 0
generated/simulator/gcc/Makefile:160: recipe for target 'build/bin/simulator.exe' failed
make[2]: *** [build/bin/simulator.exe] Error 1
generated/simulator/gcc/Makefile:155: recipe for target 'generate_assets' failed
make[1]: *** [generate_assets] Error 2
simulator/gcc/Makefile:32: recipe for target 'all' failed
make: *** [all] Error 2
Failed
Solved! Go to Solution.
2025-12-05 5:45 AM
2025-12-05 5:45 AM