cancel
Showing results for 
Search instead for 
Did you mean: 

boxProgress orientation, and circleProgress size

ksale.1
Senior II

Hi, In my UI project I need a vertucal boxProgress while all available backgrouds and images are horizontal while w&h are greyed out. When I create a custom background, the progress bar is not working. Same for circleProgress (size control). Can you help please.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Osman SOYKURT
ST Employee

Hello @ksale.1 ,

I attempted to replicate the issue but did not encounter any problems when setting up and using a vertical BoxProgress. Please verify the following two points:

  • Ensure that the height of your background image is sufficiently large.
  • In the properties panel of your BoxProgress widget (on the right side), adjust the "Appearance" setting—either up or down—according to your desired orientation. 
    OsmanSOYKURT_1-1764943423095.png

     

 

 

Osman SOYKURT
ST Software Developer | TouchGFX

View solution in original post

1 REPLY 1
Osman SOYKURT
ST Employee

Hello @ksale.1 ,

I attempted to replicate the issue but did not encounter any problems when setting up and using a vertical BoxProgress. Please verify the following two points:

  • Ensure that the height of your background image is sufficiently large.
  • In the properties panel of your BoxProgress widget (on the right side), adjust the "Appearance" setting—either up or down—according to your desired orientation. 
    OsmanSOYKURT_1-1764943423095.png

     

 

 

Osman SOYKURT
ST Software Developer | TouchGFX