cancel
Showing results for 
Search instead for 
Did you mean: 

Could not halt device (18) STM32F746G Discovery Board

jindo85547
Associate III

Hello,

I am a beginner, so forgive me if my question is basic.

I'm currently working on building a TouchGFX application that reads CAN Values and displays them on the STM32F746F Discovery Board. However, when I try to run the application, the program builds and downloads successfully before I get the error "Could not halt device (18)" and the screen on the board shows up white. 

So far, the only things that I have done to the application after generating it from TouchGFX is change the clock configuration and activate CAN1. I've attached screenshots of both in case they may be of use.

What do you think is causing the error?

Thank you.

 

jindo85547_0-1729274868587.png

jindo85547_1-1729274894296.png

 

1 ACCEPTED SOLUTION

Accepted Solutions

Sorry, by scrapping I mean I wanted to start from the beginning. I was working on Windows earlier, but I am transitioning to Linux. I'm going to try coding "by hand" for the display. 

View solution in original post

6 REPLIES 6
Karl Yamashita
Principal

Can't make out your screenshot

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

Hello @jindo85547,

Could you please explain more about your procedure and the error you are receiving? 
So, when you create a project for STM32F746G Discovery Kit from TouchGFX Designer (like the picture below), you open the STM32CubeMX project, and you apply the changes you mentioned and regenerate code from STM32CubeMX.

STM32F476G Discovery Kit Board SetupSTM32F476G Discovery Kit Board Setup

Then, do you run the application on the target from TouchGFX or do you use another method?

Mohammad MORADI
ST Software Developer | TouchGFX
GaetanGodart
ST Employee

Hello @jindo85547 ,


Have you been able to move forward on your project?

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)
jindo85547
Associate III

Sorry for the late response. I ended up scrapping and I am now trying to start from scratch on linux, but I am running into issues there. 

Hello @jindo85547 ,

 

I don't know what you mean by scrapping.

TouchGFX Designer is not supported on Linux but you can still use "plain" TouchGFX and code "by hand".

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)

Sorry, by scrapping I mean I wanted to start from the beginning. I was working on Windows earlier, but I am transitioning to Linux. I'm going to try coding "by hand" for the display.