2025-11-06 5:49 AM
Hello!
I'm working with the flexButton tool and wanted to change the color via eye-dropper. But once I turned on that option, I was unable to turn it off, I can't disable the color picker and it continously changes the color even after deselecting.
Isolating the cause a bit I realized it only happens when I move my cursor off screen into another window and click, operating the tool normally (staying within touchGFX window) correctly turns off the tool after selecting.
Just a bug I noticed,
Thank you
2025-12-04 5:13 AM
Hello @noahl.
However, I have not been able to reproduce it. I followed this procedure:
Could you share the procedure you followed if it deviates from the one described above?
I used TouchGFX 4.26.0. Which version of TouchGFX did you experience the issue in?
Best regards,
Johan