2022-02-01 6:45 AM
I m stunding TouchGFX with X-Nucleo-GFX01M1 with an example provided by STm.
In a ScreenView.cpp I can see the following code (Im will copy only one part).
void Screen1View::handleKeyEvent(uint8_t key)
{
if (animationState != ANIMATION_READY ||
menuAnimationState != MENU_ANIMATION_READY)
{
return;
}
if (key == '6')
{
// Right
menuSelectRight();where menuSelectRight is
void Screen1View::menuSelectRight()
{
menuAnimationState = MENU_ANIMATION_STEP_0;
menuAnimationTickCounter = 0;
menuAnimationDirectionLeft = false;
}menuAnimationState is just a enum and menuAnimationDirectionLeft is a boolean.
Can someone expalain where is the function to trig to go in the anohter Screen?
What I found is application().gotoLI found only I found only application().gotoSCREENNAMENoTransition();
It is in Screen1View subclass of Screen1ViewBase whitch call FrontendApplication subclass of FrontendApplicationBase
So I modify the paramter of the class Screen1View that it will read, after many jumps and inherites , from FrontendApplicationBase?
Thanks in advance
Fausto
2022-02-10 2:06 AM
Hi,
Which demo did you base this on ? need a bit more context :grinning_face_with_sweat:. Try to see if there is a GoToScreen interaction set in the Interactions tab in TouchGFX Designer.
/Romain