cancel
Showing results for 
Search instead for 
Did you mean: 

Can RAM be used for both the display frame buffer and holding dynamic bitmaps?

Andrei Chichak
Lead II

In my upcoming system I will be needing to use dynamic bitmaps.

Can dynamic bitmaps be located on the same RAM device (say SDRAM on STM32F469 discovery board) that is being used as the frame buffer?

I can carve out a piece of the SDRAM for the dynamic bitmaps, but is the DMA2D going to complain?

Thanks,

Andrei

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
LouisB
ST Employee

Hello @Andrei Chichak,

If you have enough RAM it shouldn't cause an issue, but you might have some congestion because of a lot of read and write operations on the same bus. Using different memory banks for framebuffers and dynamics bitmap can help to reduce this issue.

BR,

Louis BOUDO
ST Software Engineer | TouchGFX

View solution in original post

1 REPLY 1
LouisB
ST Employee

Hello @Andrei Chichak,

If you have enough RAM it shouldn't cause an issue, but you might have some congestion because of a lot of read and write operations on the same bus. Using different memory banks for framebuffers and dynamics bitmap can help to reduce this issue.

BR,

Louis BOUDO
ST Software Engineer | TouchGFX