cancel
Showing results for 
Search instead for 
Did you mean: 

Can I have a master screen in an application?

Karan Kolhe
Associate III

I want to use a slider which will be on master screen and then this slider can be slided/accessed on all screens in my application. I know I can add slider on every screen but is there any way to avoid that? I want to use same slider across all the screens. And also Date name and all that is common for every screen like status bar in phones

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Martin KJELDSEN
Chief III

Yes you can. The designer doesn't support this, but it could in the future - Basically, what you're forced to do is to have something like a Custom Container in every view and then some code replicated by the presenter for that concrete view.

In your case, you could have a custom container that has all the elements you want, but the presenter method to update those elements through the view from the model would have to be replicated.

To have a BASE-VIEW and BASE-PRESENTER for a group of screens you would have to create a new class by hand that you can then inject in between the designer-generated view and your inherited view for that generated base view.

I'm swamped - I promised i'd do an example for someone else and it's still on my list!

/Martin

View solution in original post

1 REPLY 1
Martin KJELDSEN
Chief III

Yes you can. The designer doesn't support this, but it could in the future - Basically, what you're forced to do is to have something like a Custom Container in every view and then some code replicated by the presenter for that concrete view.

In your case, you could have a custom container that has all the elements you want, but the presenter method to update those elements through the view from the model would have to be replicated.

To have a BASE-VIEW and BASE-PRESENTER for a group of screens you would have to create a new class by hand that you can then inject in between the designer-generated view and your inherited view for that generated base view.

I'm swamped - I promised i'd do an example for someone else and it's still on my list!

/Martin