cancel
Showing results for 
Search instead for 
Did you mean: 

Can anyone suggest me 8" to 10" TFT LCD + Capacitive Touch screen with MIPI DSI interface which can be directly connected to STM32F469I-Discovery Board?

SK S.1
Associate III

Hi Guys,

I want to connect 8" to 10" TFT LCD + Capacitive Touch Screen display with MIPI DSI interface to STM32F469I-Discovery just by removing the existing 4" TFT LCD. I had searched in the internet and I didn't get any TFT LCD CTP with MIPI DSI interface which can be directly connect to STM32F469I-Discovery board. STM32F469I-Discovery board uses 25 pin connector (CN10) for LCD and 6 pin connector (CN2) for Capacitive Touch screen.

Can anyone suggest me 8" to 10" TFT LCD + Capacitive Touch screen with MIPI DSI interface which can be directly connected to STM32F469I-Discovery Board?

With Regards

SUNIL K S

Ace Designers Ltd

This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11

​Hi,

Thanks for the suggestion.

With Regards

Sunil K S

SKacp.1
Senior II

Hi,

I have ordered TFT LCD  PH720128T003-ZBC02. I plan to connect with STM32MP1 (module VisionSOM-STM32MP1 company SOMLabs) https://somlabs.com/product/visionsom-stm32mp1/. I have also plan to connect with STM32F769 or STM32H74x.