cancel
Showing results for 
Search instead for 
Did you mean: 

Building a project on newer touchgfx 4.13.0 which was developed on touchgfx 4.8.0 creates distortion on images.

FShai.11
Associate II

We have our hardware which was developed and built on an older version of touchgfx (4.8.0). We are trying to build the same project with the newer touchgfx (4.13.0). When we do so, there are some small distortion on the images. How do we solve this?

2 REPLIES 2
Martin KJELDSEN
Chief III

Screenshots etc, please :) Did you try to diff the two projects to see if the upgrade process went as expected?

/Martin

Thank you for replying.

This is the screen looks like. Distorted, having dots all around with new build.

0693W000001rQH3QAM.jpg

-Faizal