cancel
Showing results for 
Search instead for 
Did you mean: 

BUG on touch GFX4.20.0

MDi D.1
Associate II

If you choose the object "Static Graph"

and in this order:

set Y-axis Range Min = 60

set X-axis Range Min = 0

set X-axis Range Max = 8

click with the mouse into the Y-axis Range Min box

The value into the X-axis Range Max change itself at 60.0001 and is impossible to set again the correct value.

For us is a big problem.

Thanks Marco

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
wired
Senior III

The Great Carnac predicts a 4.20.1 release being issued soon. X-max is being compared against Y-min instead of X-min. That could cause a lot of problems. The fact that this has been undetected until now tells me how many people are actually using the static graph (at least in the Designer).