cancel
Showing results for 
Search instead for 
Did you mean: 

Black Screen after 4-5 Reboot

Ngard.1
Associate

Hello,

I'm using STM32H750IB (touchgfx 4.13.0 with freertos  V10.2.1) to control RGB TFT LCD, with external flash and also external SDRAM.

The application runs well but sometimes (after 4-5 reboot) the screen remains black, if I reboot the application starts correctly.

After some tests I found that the LTDC module goes in FIFO UNDERRUN when the black screen happens. SDRAM is initialize in the bootloader and the LTDC is initialize in the application.

How can I solve this problem?

Best Regards

Nicola

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Martin KJELDSEN
Chief III

I'm not sure why it would happen after 4-5 reboots. Try reducing the pixel clock a bit to see if you're still having that issue. Or using hal.lockDMAToFrontPorch(true); in your TouchGFXHAL.cpp (initialize()).

This will overall reduce the strain on your memory bus.

 /Martin