cancel
Showing results for 
Search instead for 
Did you mean: 

ApplicationTemplate for STM32F469I DiscoveryKit

AKrug
Associate II

ApplicationTemplate for STM32F469I DiscoveryKit create Keil project file for uVision v4 with wrong TargetOption. <Device>STM32F427ZI</Device>. Where i can get right ApplicationTemplate for STM32F469I DiscoveryKit ?

Thanks.

4 REPLIES 4
Martin KJELDSEN
Chief III

Hi @AKrug​,

You're right about the device type. What happens if you change to the proper device type? Are you able to program your board?

If I use only TouchGFX designer and Visual Studio there is no problem.

All Designers modes (Simulate, Run, Generate ) works without problem.

Visual Studio compile and run Simulator.

Problems begin if I try open Keil project file. It causes a storm of indignation from keil.

Replacing the device type does not give results.

As I understand it is necessary to make much more changes to the Keil project file.

Before, I didn’t use Keil so I asked where to get the working version of Application Template.

Can you send me the correct Keil project file for this ApplicationTemplate?

Hi,

Yes, Touchgfx designer uses arm-gcc to create a binary and ST-Link to program. I think there is a general issue with the Keil project for this particular application template that has escaped testing - I will investigate and get back to you.

Best regards,

Martin

Thank you for attention.

I look forward to your reply.

Best regards,

Andrew