‎2019-05-31 10:31 PM
‎2019-06-03 1:22 AM
Hi @KMitt​,
Can you please attach your log file?
/Martin
‎2019-06-03 5:16 AM
Thanks for the reply...there was no log file generated because it can't load the template. It finally worked when I changed the directory location.
Can you put links for tutorials on modifying the code for adding different buttons (especially sliders).
Also what type of compiler will be good if I don't have visual studio
‎2019-06-06 4:36 AM
Hi,
If you don't have visual studio TouchGFX comes with gcc projects out of the box. (Also available if you create your TouchGFX projects through CubeMX/CubeIDE).
I suggest you check out these resources to get started with adding widgets: https://touchgfx.zendesk.com/hc/en-us/categories/200529271
/Martin
‎2019-06-11 4:41 AM
Hi @KMitt​,
Any progress on this?
/Martin
‎2019-06-17 7:40 AM
Thanks for the reply. I checked the tutorials but it is not much help.
Can you tell me how to use input from slider button for changing the text fields.
Kumud
‎2019-07-23 7:39 AM
Hello
Can you look into this. The slider button is causing problems. I think the issue is from software side
please check
‎2019-08-05 5:52 AM
You have no background.
‎2019-08-05 5:53 AM
Just back from vacation now, sorry for the late reply. When the knob leaves an area of the screen because you're dragging what's left behind must be redrawn - But there's nothing there.