2021-07-30 5:59 AM
Upon entering a screen which contains a swipe container 'sub_settings_swipe_container' I'm performing some logic based on where the screen is getting it's brightness from. Either manually set via a scrollwheel elsewhere or through a CAN message.
void sub_settings_swipeView::setupScreen()
{
sub_settings_swipeViewBase::setupScreen();
sub_settings_swipe_container.setSelectedPage(navigate_to_screen != 0xff ? navigate_to_screen : 0);
current_page = sub_settings_swipe_container.getSelectedPage();
// Global_Settings_2_2
switch(FFC.brightness_source)
{
case can_source:
can_button.setSelected(true);
manual_button.setSelected(false);
sub_settings_swipe_container.add(sub_1_settings_1);
sub_settings_swipe_container.add(sub_1_settings_2);
sub_settings_swipe_container.setPageIndicatorXY(98, 212);
// Global_Settings_2_4
CAN_brightness_scroll_wheel.animateToItem(ceil((FFC.CAN_Backlight_Adjust*100)-50), 3);
CAN_brightness_scroll_wheel.invalidate();
can_found.setVisible(true);
can_not_found.setVisible(false);
can_found.invalidate();
can_not_found.invalidate();
break;
case manual_source:
can_button.setSelected(false);
manual_button.setSelected(true);
sub_settings_swipe_container.remove(sub_1_settings_1);
sub_settings_swipe_container.remove(sub_1_settings_2);
sub_settings_swipe_container.setPageIndicatorXY(113, 212);
break;
}
can_button.invalidate();
manual_button.invalidate();
sub_settings_swipe_container.invalidate();
}Upon entering this screen... I look at what is saved to memory, the switch/case statement on FFC.brightness_source, and populate the screen accordingly. The issue is, when I enter this screen and the source is set to can_source, the code dies at the step where I go to add(sub_1_settings_1).
However, if the brightness source is set to manual, it removes these screens just fine, and then I can toggle them on/off with the can_button/manual_button radio buttons. This is handled in the handleTickEvent()
void sub_settings_swipeView::handleTickEvent()
{
previous_page = current_page;
current_page = sub_settings_swipe_container.getSelectedPage();
switch(current_page)
{
case sub_1_settings_page_0:
previous_brightness_source = brightness_source;
if(can_button.getSelected())
brightness_source = can_source;
else
brightness_source = manual_source;
if(brightness_source != previous_brightness_source)
{
switch(brightness_source)
{
case can_source:
sub_settings_swipe_container.add(sub_1_settings_1);
sub_settings_swipe_container.add(sub_1_settings_2);
sub_settings_swipe_container.setPageIndicatorXY(98, 212);
break;
case manual_source:
sub_settings_swipe_container.remove(sub_1_settings_1);
sub_settings_swipe_container.remove(sub_1_settings_2);
sub_settings_swipe_container.setPageIndicatorXY(113, 212);
break;
}
sub_settings_swipe_container.invalidate();
}
break;To reiterate, the adding/removing of screens works in the handleTickEvent(), but adding screens dies in the setupScreen function. Any tips or advice?
Thanks,
Ryan
Solved! Go to Solution.
2021-07-30 7:12 AM
Seems as your sub settings exist and is added in screen base then you cant add it in setup, but you can remove.
2021-07-30 7:12 AM
Seems as your sub settings exist and is added in screen base then you cant add it in setup, but you can remove.
2021-07-30 7:37 AM
Thank you MM..1! I removed the .add(sub_1_settings_1) and add(sub_1_settings_2) and that fixed the issue I was seeing! Not sure what I was thinking when I thought those needed to be there. Like you said, those screens are already included in the base when the screen was setup.
Much appreciated!