2019-10-21 2:32 AM
Hi together,
I have a tinker board with a STM32F405RG (1024kB Flash 192kB SRAM, no FMC, no DMA2D) and an EADOGXL Display (SPI, 240x128, 4bit Grey).
As of now i've only played with the 'baremetal' data and command to the display.
I am wondering what the actual hw requirements for a custom board in touchgfx are.
Is the DMA2D (ChromART) required?
It says so in the Getting started with cubemx https://touchgfx.zendesk.com/hc/en-us/articles/360020001492-Getting-Started-with-CubeMX-and-TouchGFX
I plan to use a single (or double) frambuffer in internal Memory, as it is a greyscale display with a not to high resolution it should be 240*128*4bit = 15kB of SRAM.
Am I missing something else?
Btw is there any full toturial on how to create your own target/board from scratch?
Thanks in advance
Solved! Go to Solution.
2019-10-21 4:55 AM
Hi @a.lex,
Actually, you do not need much to run TouchGFX. If we take something simple and low cost to exemplify you could run TouchGFX on a G0 in internal RAM using a partial framebuffer strategy displaying on a SPI display.
You do not need DMA2D.
You do not need external RAM.
You do not need external FLASH.
But, you need to tailor your hardware to your UI requirements, of course. E.g.
/Martin
2019-10-21 4:55 AM
Hi @a.lex,
Actually, you do not need much to run TouchGFX. If we take something simple and low cost to exemplify you could run TouchGFX on a G0 in internal RAM using a partial framebuffer strategy displaying on a SPI display.
You do not need DMA2D.
You do not need external RAM.
You do not need external FLASH.
But, you need to tailor your hardware to your UI requirements, of course. E.g.
/Martin
2019-10-21 8:54 AM
Hi Martin,
Thank you very much, this is enough for me to give it a try.
I think initially configuring it via cube mx (as my mcu does not have an dma2d) is not possible, so I will start from scratch.
Is there a minimalist example available? Like only rendering into a small frame buffer on the chip?
Br,
Alex
2019-10-23 2:01 PM
I guess there's not something like you're describing - It's quite sad that CubeMX has these restrictions today so that you can only use TouchGFX with an LTDC/DSI/SDRAM/QSPI because that's what most of the the stm32 based boards were supporting when the integration was first started - To sort of lock in the combinations of IPS that were known to be "good".
We're working on something that will allow you to do just what you're describing. For any MCU, simply enable TouchGFX and render frames into some memory (But allows you to do much more complex things of course). It won't be ready until end 2019
Most of our application templates are made like that - from scratch, not using CubeMX (but CubeFW), so check those out and let me know if that can give yuo some inspiration.
/Martin