TouchGFX shows flicker on content update
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-07-01 7:18 AM
Hi
we had made a custom STM32 board and we had some issues setting up TouchGFX.
Display parallel interface with 800 x 480 pixels Model - > AT070TN94
MCU: STM32H7B0VBT6
External Flash QuadSpi W25Q128JV
I use external Flash Boot Loader
LDTC Clock 32MHz
The images are displayed well until they are updated, but after the update, they have problems. The problem can be seen in the video below.
0 REPLIES 0