2022-10-17 2:07 AM
Hi,
My custom SBSFU_UserApp.bin failed the header signature verification in slot SLOT_ACTIVE_1 when I tried to execute it on the STM32H7B3I-DK board.
To replace ECDSA with RSA signing verification, I have changed se_crypto_bootloader.c.
SECoreBin project's se_crypto_bootloader.c file needs to be debugged.
I am using STM32Cube IDE and compiling the applications as per the order mention in the readme file of the STM32H7B3I-DK 1_Image demo project.
Please let me know, what is the debug mechanism for SECoreBin application? How can I enable debug mode of SBSFU Secure Engine application?
Thanks,
2022-10-19 7:27 AM
I am faced the Same Situation over my working, But it resolved after some time automatically.