cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U585 SBSFU - Can't invoke external loader in production mode

horatiosdad
Associate II

 

After porting the application "STM32Cube_FW_U5_V1.8.0\Projects\B-U585I-IOT02A\Applications\SBSFU" to our own board we have everything operational apart from the ability to invoke the local loader in production mode (RDP2).

I have reverted to the original B-U585I-IOT02A board and project and have a similar issue so I am wondering if this is broken or we have misunderstood something. The loader can be invoked in TFM_DEV_MODE with RDP0 but not in production mode with RDP2. The SBSFU application runs fine.

Changes from the default STM SBSFU project settings we used to test this on B-U585I-IOT02A

1) In SBSFU_Boot project remove the TFM_DEV_MODE pre-processor symbol definition

2) In boot_hal_cfg.h >> #define TFM_TAMPER_ENABLE NO_TAMPER

3) In boot_hal_cfg.h >> #define #define TFM_OB_BOOT_LOCK 0

4) In flash_layout.h >> //#define MCUBOOT_PRIMARY_ONLY (definition commented out)

5) In flash_layout.h >> #define MCUBOOT_APP_IMAGE_NUMBER 2

6) In hardening.sh >> write_protect_secure="-ob...........BOOT_LOCK=0"

 

Any ideas?

Thanks in advance

 

2 REPLIES 2
Jocelyn RICARD
ST Employee

Hello @horatiosdad ,

that is strange indeed.

To jump in the loader you use the user button after a reset ?

Then what happens ?

Did you try re-enabling the traces ?

Best regards

Jocelyn

 

Hi @Jocelyn RICARD 

Pressing the user button over a reset prevents the application from running. The LED doesn't flash and the ns-appli menu is not output.

 

Enabling logging results in the following single line 

[INF] Flash operation: Op=0x0, Area=0x0, Address=0x0\r\n