STM32H523RCT6 READ OUT PROTECTION LEVEL1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-10-06 11:08 PM
Hi ST Team,
Currently i am using STM32H523RCT6 mcu for one of my project.
In this i want to set the read out protection of level 1.
Currently i am using below sequence to set the read out protection of level 1 protection..
// Unlock the flash option bytes
HAL_FLASH_Unlock();
// Set the read out protection level to Level 1
// RDP Level 1 is indicated by the value 0x01
uint32_t option_bytes = 0x01; // RDP Level 1
HAL_FLASH_OB_Unlock();
// Program the option byte
HAL_FLASHEx_OBProgram(&option_bytes);
// Start the option byte change
//HAL_FLASH_OB_Launch();
// Lock the option bytes
HAL_FLASH_OB_Lock();
// Lock the flash memory
HAL_FLASH_Lock();
HAL_FLASH_OB_Launch();
but this is not working.....
So can you please send me a sample code or routine to set the read out protection of level 1.
Thanks with Regards,
DEEPAK
Labels:
- Labels:
-
STM32H5 Series
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-10-07 5:51 AM
Hello @DeepakKumar ,
There is a "Product State" feature available on STM32H5 which functions similar to the readout protection (RDP) feature.
Please refer to these articles :
- How to enable RDP-like product state flash protect... - STMicroelectronics Community
- Security:Product state for STM32H5 - stm32mcu
This workshop video presents the new mechanism of readout protection introduced in STM32H5:
When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Thanks
Imen