cancel
Showing results for 
Search instead for 
Did you mean: 

Since the SBSFU doesn't work for all processors, is there a document on how a secure boot process would work with the TPM chip as the root of trust entity?

WTom
Associate III
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Jocelyn RICARD
ST Employee

Hello,

the next release of SBSFU coming in July will have the ability to connect to ST's STSafe which is a secure element dedicated to IOT.

No TPM interfacing is planned because TPM is overkill for such application.

The SBSFU can be ported on any STM32 processor.

Next release will support other STM32 families such as L0, L1, G4, WB.

F0, F1, F2, and F3 are not supported in the package but a poring could be done

Best regards

Jocelyn

View solution in original post

2 REPLIES 2
Jocelyn RICARD
ST Employee

Hello,

the next release of SBSFU coming in July will have the ability to connect to ST's STSafe which is a secure element dedicated to IOT.

No TPM interfacing is planned because TPM is overkill for such application.

The SBSFU can be ported on any STM32 processor.

Next release will support other STM32 families such as L0, L1, G4, WB.

F0, F1, F2, and F3 are not supported in the package but a poring could be done

Best regards

Jocelyn

WTom
Associate III

Thanks....looking forward to the next SBSFU release and the new info.