cancel
Showing results for 
Search instead for 
Did you mean: 

RDP level 1 flash protection on STM32H753

YROSS
Associate II

Hello,

When the RDP level 1 protection option bytes is set and the boot adress is set in the user flash memory, what are the debugger protections ? Which parts of the microcontroller still remain available via the JTAG debug port or the SWD debug port ?

are the debugger protections the same with a boot adress in system memory (ST embedded bootloader ) ?

Thanks

Yves

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0