2021-09-28 7:35 AM
Is there any configuration we need to modify in prepareimage.py to overcome this error "ERROR: overlapped zone is not empty" or any other configuration?
Below is output.txt file.
python /Users/username/Downloads/STM32Cube_FW_WL_V1.1.0/Middlewares/ST/STM32_Secure_Engine/Utilities/KeysAndImages/prepareimage.py
block size =16
Magic: SFU2!!
Magic: SFU2!!
header 0x0803F000
merge: python /Users/username/Downloads/STM32Cube_FW_WL_V1.1.0/Middlewares/ST/STM32_Secure_Engine/Utilities/KeysAndImages/prepareimage.py mergev2 -v 0 -e 1 -b ../../../STM32CubeIDE/Binary/SBSFU_LoRaWAN_End_Node_DualCore_CM0Plus.bin@0x801f200;../../../STM32CubeIDE/Binary/LoRaWAN_End_Node_DualCore_CM4sfuh.bin@0x0803F000 -f ../../../../2_Images_SBSFU/STM32CubeIDE/CM4/Debug/SB.elf;./LoRaWAN_End_Node_DualCore_CM4.elf ../../../STM32CubeIDE/Binary/SBSFU_LoRaWAN_End_Node_DualCore_CM4.bin
number of segment :4
0x8000138
0x80016a0
0x80016b0
Adding ELF file: ../../../../2_Images_SBSFU/STM32CubeIDE/CM4/Debug/SB.elf from 0x8000000 to 0x80016b0
number of segment :5
0x8019ccc
0x8019d2c
0x8019d30
0x8019d30
Adding ELF file: ./LoRaWAN_End_Node_DualCore_CM4.elf from 0x8013200 to 0x8019d30
Adding BIN file: ../../../STM32CubeIDE/Binary/SBSFU_LoRaWAN_End_Node_DualCore_CM0Plus.bin from 0x801f200 to 0x803fa00
Adding BIN file: ../../../STM32CubeIDE/Binary/LoRaWAN_End_Node_DualCore_CM4sfuh.bin from 0x803f000 to 0x803f200
ERROR: overlapped zone is not empty
python /Users/username/Downloads/STM32Cube_FW_WL_V1.1.0/Middlewares/ST/STM32_Secure_Engine/Utilities/KeysAndImages/prepareimage.py mergev2 -v 0 -e 1 -b ../../../STM32CubeIDE/Binary/SBSFU_LoRaWAN_End_Node_DualCore_CM0Plus.bin@0x801f200;../../../STM32CubeIDE/Binary/LoRaWAN_End_Node_DualCore_CM4sfuh.bin@0x0803F000 -f ../../../../2_Images_SBSFU/STM32CubeIDE/CM4/Debug/SB.elf;./LoRaWAN_End_Node_DualCore_CM4.elf ../../../STM32CubeIDE/Binary/SBSFU_LoRaWAN_End_Node_DualCore_CM4.bin : failedPlease advise.
2021-09-30 6:36 PM
Would be great if any help on this issue. Any one facing same issue?
2021-09-30 9:24 PM
Build on macOS have some bug(s) as I could see all perfectly working fine on Windows 10. Basically, the issue is UserApp is not executing at all when you compile in macOS version of STM32CubeIDE.