Not able to start time 7 as interrupt in bootloader
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-14 5:34 AM
I am using STM32L562-DK for my development, I am using SBSFU.
In bootloader, I want to use timer 7 as an interrupt. I am configuring it as following
TIM_HandleTypeDef htim7;
void TIM7_IRQHandler(void)
{
/* USER CODE BEGIN TIM6_IRQn 0 */
/* USER CODE END TIM6_IRQn 0 */
HAL_TIM_IRQHandler(&htim7);
/* USER CODE BEGIN TIM7_IRQn 1 */
/* USER CODE END TIM7_IRQn 1 */
}
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
/* USER CODE BEGIN Callback 0 */
/* USER CODE END Callback 0 */
if (htim->Instance == TIM7) {
printf("\r\n TIM7 Callback");
}
/* USER CODE BEGIN Callback 1 */
/* USER CODE END Callback 1 */
}
HAL_StatusTypeDef Boot_StartWatchdgFeedTimer(void)
{
RCC_ClkInitTypeDef clkconfig;
uint32_t uwTimclock = 0;
uint32_t uwPrescalerValue = 0;
uint32_t pFLatency;
/*Configure the TIM7 IRQ priority */
HAL_NVIC_SetPriority(TIM7_IRQn, 0 ,0);
/* Enable the TIM7 global Interrupt */
HAL_NVIC_EnableIRQ(TIM7_IRQn);
/* Enable TIM7 clock */
__HAL_RCC_TIM7_CLK_ENABLE();
/* Get clock configuration */
HAL_RCC_GetClockConfig(&clkconfig, &pFLatency);
/* Compute TIM7 clock */
uwTimclock = HAL_RCC_GetPCLK1Freq();
/* Compute the prescaler value to have TIM7 counter clock equal to 1MHz */
uwPrescalerValue = (uint32_t) ((uwTimclock / 1000000U) - 1U);
printf("\r\n uwTimclock = %d\r\n",uwTimclock);
printf("\r\n uwPrescalerValue = %d",uwPrescalerValue);
/* Initialize TIM7 */
htim7.Instance = TIM7;
/* Initialize TIMx peripheral as follow:
+ Period = [(TIM7CLK/1000) - 1]. to have a (1/1000) s time base.
+ Prescaler = (uwTimclock/1000000 - 1) to have a 1MHz counter clock.
+ ClockDivision = 0
+ Counter direction = Up
*/
htim7.Init.Period = (1000000U / 1000U) - 1U;
htim7.Init.Prescaler = uwPrescalerValue;
htim7.Init.ClockDivision = 0;
htim7.Init.CounterMode = TIM_COUNTERMODE_UP;
if(HAL_TIM_Base_Init(&htim7) == HAL_OK)
{
/* Start the TIM time Base generation in interrupt mode */
printf("\r\nTImer Start Ret valur\n");
int ret = HAL_TIM_Base_Start_IT(&htim7);
printf("\r\nTImer Start Ret value = %d\r\n",ret);
return ret;
}
/* Return function status */
return HAL_ERROR;
}
My code is hanging after executing HAL_TIM_Base_Start_IT() API, I have declared void TIM7_IRQHandler(void) in boot_hal.h, and all above APIs are written in boot_hal.c.
Is there any specific configuration required to use tim7 as an interrupt in the bootloader?
I have tried with timer 6, code is not hung HAL_TIM_Base_Start_IT() with timer 6 but the interrupt was not generated.
@Frantz LEFRERE​ , Can you please help me regarding it?
- Labels:
-
Bootloader
-
STM32L5 Series
-
X-Cube-SBSFU
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-15 12:49 AM
Is there any MPU protection I need to check?
With TIM6 firmware does not hang but interrupt is not generated. I have checked the counter value of TIM6 which has been increasing, resetting, and starting from 0 again, But the interrupt is not generated.
In TIM6 and TIM7 registers values are the same as below before calling HAL_TIM_Base_Start_IT() API
CR1 = 0
CR2 = 0
DIER = 0
SR = 1
EGR = 0
@Frantz LEFRERE​ , Have you tested on STM32L562E-DK?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-15 4:09 AM
Test done on a Nucleo with the ST delivered code.
I don't think MPU would have an impact but to check put the call with a while(1) loop before TFM_LL_SECU_ApplyRunTimeProtections
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-15 10:44 PM
Please check the NVIC->ITNS register and insure the interrupt properly assigned to secure or non-secure regarding your code.
By default all the IRQ are secure, setting a bit to one, assign the IRQ to non-secure.
You can try to generate example code with CubeMX and check
Usually configuration is done in the TZ_SAU_Setup :
#if defined (NVIC_INIT_ITNS0) && (NVIC_INIT_ITNS0 == 1U)
NVIC->ITNS[0] = NVIC_INIT_ITNS0_VAL;
#endif
#if defined (NVIC_INIT_ITNS1) && (NVIC_INIT_ITNS1 == 1U)
NVIC->ITNS[1] = NVIC_INIT_ITNS1_VAL;
#endif
#if defined (NVIC_INIT_ITNS2) && (NVIC_INIT_ITNS2 == 1U)
NVIC->ITNS[2] = NVIC_INIT_ITNS2_VAL;
#endif
#if defined (NVIC_INIT_ITNS3) && (NVIC_INIT_ITNS3 == 1U)
NVIC->ITNS[3] = NVIC_INIT_ITNS3_VAL;
#endif
Thanks flag define in partition_stm32l552xx.h
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-16 1:20 AM
Value of NVIC->INTS is as below
NVIC->ITNS[0] = 00
NVIC->ITNS[1] = 00
NVIC->ITNS[2] = 00
NVIC->ITNS[3] = 00
NVIC->ITNS[4] = 00
NVIC->ITNS[5] = 00
NVIC->ITNS[6] = 00
NVIC->ITNS[7] = 00
NVIC->ITNS[8] = 00
NVIC->ITNS[9] = 00
NVIC->ITNS[10] = 00
NVIC->ITNS[11] = 00
NVIC->ITNS[12] = 00
NVIC->ITNS[13] = 00
NVIC->ITNS[14] = 00
NVIC->ITNS[15] = 00
In my application, if I write the same code It is working, But it is not working in the bootloader.
One thing I have found is that currently, FLASH_AREA_PERSO_SIZE size is 0x900, if I change it to 0x800 interrupt is generated and working. But bootloader is not able to jump into the application after changing FLASH_AREA_PERSO_SIZE macro to 0x900 due to a size issue.
What is the relation between FLASH_AREA_PERSO_SIZE and TIM7 interrupt?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-16 2:48 AM
Modifying the FLASH_AREA_PERSO_SIZE , should modify the boot address please insure you properly align SECBOOTADD0

- « Previous
-
- 1
- 2
- Next »