cancel
Showing results for 
Search instead for 
Did you mean: 

AES-CCM Tag gives wrong values

Keerthi
Associate III

Hi,

 

I am working on the STM32H533RE microcontroller and implementing AES-CCM encryption using a NIST test vector for validation. While the encrypted output matches the expected result, the authentication tag generated is incorrect. I have shared the relevant code and configuration above for reference.

CRYP_HandleTypeDef hcryp; uint32_t pKeyAES[4] = {0x40414243,0x44454647,0x48494A4B,0x4C4D4E4F}; __ALIGN_BEGIN static const uint8_t HeaderAES[16] __ALIGN_END = { 0x00, 0x08, // Length = 8 bytes 0x00, 0x01, 0x02, 0x03, // AAD 0x04, 0x05, 0x06, 0x07, 0x00, 0x00, 0x00, 0x00, // Padding 0x00, 0x00 }; __ALIGN_BEGIN static const uint32_t B0AES[4] __ALIGN_END = { 0x4f101112,0x13141516,0x00000000,0x00000004}; uint8_t sampledata[4] = {0x20, 0x21, 0x22, 0x23}; uint8_t sampleoutputdata[8]; uint32_t sampletagdata[8]; // 4 bytes static void MX_AES_Init(void) { /* USER CODE BEGIN AES_Init 0 */ /* USER CODE END AES_Init 0 */ /* USER CODE BEGIN AES_Init 1 */ /* USER CODE END AES_Init 1 */ hcryp.Instance = AES; hcryp.Init.DataType = CRYP_BYTE_SWAP; hcryp.Init.KeySize = CRYP_KEYSIZE_128B; hcryp.Init.pKey = (uint32_t *)pKeyAES; hcryp.Init.Algorithm = CRYP_AES_CCM; hcryp.Init.Header = (uint32_t *)HeaderAES; hcryp.Init.HeaderSize = 4; hcryp.Init.B0 = (uint32_t *)B0AES; hcryp.Init.DataWidthUnit = CRYP_DATAWIDTHUNIT_BYTE; hcryp.Init.HeaderWidthUnit = CRYP_HEADERWIDTHUNIT_BYTE; hcryp.Init.KeyIVConfigSkip = CRYP_KEYIVCONFIG_ALWAYS; hcryp.Init.KeyMode = CRYP_KEYMODE_NORMAL; if (HAL_CRYP_Init(&hcryp) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN AES_Init 2 */ /* USER CODE END AES_Init 2 */ } main() { HAL_CRYP_Encrypt(&hcryp, sampledata, 4, sampleoutputdata, 1000); HAL_CRYPEx_AESCCM_GenerateAuthTAG(&hcryp, sampletagdata, HAL_MAX_DELAY); }
View more

 

1 REPLY 1
Keerthi
Associate III

Hi,

 

Could someone help me what is the issue which generating the tag value for the AES-CCM. Thanks in advance