2017-10-26 7:51 AM
hi, I have a stm32l476 necleo-64 board and CCA02M1 extension board. I want to modify the the Microphones_Streaming example. and I want to use it to record 4 channel microphone and with 48000Hz sample rate. and I just change the macro definition AUDIO_CHANNELS in the aduio_application.h. change the 2 to 4
&sharpdefine AUDIO_CHANNELS 2 ------------> 4
but the Audacity didn't work after the change,it reprot error like this
and the the same thing happens when I change the AUDIO_SAMPLING_FREQUENCY to 48000
and I think mabe I should change the USB descripter at the same time, but how to modify it ?
#microphones_streaming #stm32l476 #cca02m12017-10-26 1:30 PM
>>
I think maybe I should change the USB descriptor at the same time, but how to modify it ?
There are perhaps specification documents that might be enlightening..
2017-11-15 1:09 AM
Hello,
You need to change the sittings of you'rerecording device on windows: Audio sampling frequency and Audio channels.
2018-01-31 4:30 AM
Hey, Zhangyi, have you managed to change the code? I'm facing the same issue. You probably have to change some code in the USB driver and solder/unsolder some resistors in the X-NUCLEO board. I'm okay with the soldering stuff, but the coding is driving me nuts hehe
2018-06-01 3:01 AM
Hello I need your help, I work with stm32f401RE, I would like to do the project Microphones_Streaming and after doing the LS_application ''localization source'', I did not use the x-nucleo-cca02m1 but I did a montage paraille, I know why my pc does not even detect the door of the acquisition, and because of the mounting X-nucleo-cca02m1 thank you