cancel
Showing results for 
Search instead for 
Did you mean: 

X-CUBE-MCSDK 5.0.2 can not be installed ! ( 32 and 64 bits )

gokay aygok
Associate III
Posted on April 15, 2018 at 14:41

Hello dear stm32 community !

Since yesterday, I have been trying to install X-CUBE-MCSDK 5.0.2. However, I am having some problems. On my computer with 32 bits, the error is, program is too big to fit in memory. On my other computer with 64 bits, the error is, the file is not compatible with windows version ( I have tried in windows 10 and 7 with 64 bits).

Could you please help me install and find out how to fix the problems ?

Or can someone share with me older versions of X-CUBE-MCSDK 5.0.2 such as 5.0.0 or 5.0.1 ? ( would be great ! )

Any answer and help attempt is appreciated !

Thank you so much in advance...

Best regards...

#64bits #sdk-foc #x-cube-mcsdk-5.0.2 #32bits #stm32-mc-pmsm-sdk #sdk
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
gokay aygok
Associate III
Posted on April 16, 2018 at 11:50

I have solved the problem. Hopefully, users with the same problem can install the program easily.

Tu run the exe(setup)file properly, just right click on the exe file. Then open it with Winrar. There you go, installing will start.

View solution in original post

1 REPLY 1
gokay aygok
Associate III
Posted on April 16, 2018 at 11:50

I have solved the problem. Hopefully, users with the same problem can install the program easily.

Tu run the exe(setup)file properly, just right click on the exe file. Then open it with Winrar. There you go, installing will start.