cancel
Showing results for 
Search instead for 
Did you mean: 

Why is my current comsumption much higher in standby than what is mentionned in the Datasheets

*Steve*
Associate

Hello guys,

I've been trying to enter the Standby Mode using the Exemples from st and i got it work. But in Standby i'm still around 6mA.

This is much more than the expected 5 µA! Maybe someone knows what may cause this Behaviour?

thank you for your help!

/*My Code*/

#define PWR_WAKEUP_PIN_FLAGS (PWR_WAKEUP_FLAG1 | PWR_WAKEUP_FLAG2 | PWR_WAKEUP_FLAG3 | PWR_WAKEUP_FLAG4 | PWR_WAKEUP_FLAG5 | WR_WAKEUP_FLAG6)

void vtest2(void* Param)

{

 /* Check and handle if the system was resumed from StandBy mode */

 if(__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET)

 {

  /* Clear Standby flag */

  __HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB_D1);

  __HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB_D2);

  __HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);

  __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);

  __HAL_PWR_CLEAR_FLAG(PWR_WAKEUP_PIN_FLAGS);

 }

 /*Disablke WakeUp Pin*/

 HAL_PWREx_DisableWakeUpPin(PWR_WAKEUP_PIN4);

 /* Clear all related wakeup flags */

 HAL_PWREx_ClearWakeupFlag(PWR_WAKEUP_FLAG4);

 PWREx_WakeupPinTypeDef sPinParams;

 /* Enable WakeUp Pin PWR_WAKEUP_PIN4 connected to PC13*/

 sPinParams.WakeUpPin  = PWR_WAKEUP_PIN4;

 sPinParams.PinPolarity = PWR_PIN_POLARITY_HIGH;

 sPinParams.PinPull   = PWR_PIN_NO_PULL;

 HAL_PWREx_EnableWakeUpPin(&sPinParams);

/*Enter Standby*/

 HAL_PWREx_EnterSTANDBYMode(PWR_D1_DOMAIN);

HAL_PWREx_EnterSTANDBYMode(PWR_D2_DOMAIN);

HAL_PWREx_EnterSTANDBYMode(PWR_D3_DOMAIN);

HAL_PWREx_ConfigD3Domain(PWR_D3_DOMAIN_STOP);

HAL_RCC_DeInit();

HAL_PWR_EnterSTANDBYMode();

while_(1)

{

}

}

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0