Skip to main content
MBelk
Associate II
September 15, 2019
Solved

I want to get gpio clock by passing data into GPIO_BSRR registers by DMA transaction on capture compare timer event. It doesn't work.

  • September 15, 2019
  • 7 replies
  • 1350 views

My timer config:

  RCC_APB1ENR = RCC_APB1ENR_TIM3EN;

  TIM3_CR1 = (uint32_t)(TIM_CR1_CKD_CK_INT | TIM_CR1_CMS_CENTER_3);

  TIM3_CR1 &= ~TIM_CR1_UDIS;

  TIM3_CR2 &= ~TIM_CR2_CCDS;

  TIM3_ARR = (uint32_t)10000;

  TIM3_DIER = (uint32_t)(TIM_DIER_CC1DE | TIM_DIER_CC1IE);

  PWM_BORDER = (uint32_t)7000;

So, timer interrupt is working well only when I null CCR event in the interupt.

But transaction interrupt arises at random moments of time. While transacion must takes few SysClk's. May be I have wrong timer config of timer or wrong DMA channel?

DMA config:

  RCC_AHBENR |= RCC_AHBENR_DMA1EN;

  DMA1_CPAR4 = (uint32_t) &GPIOF_BSRR;

  DMA1_CMAR4 = (uint32_t) &clockSeq;

  DMA1_CNDTR4 = (uint32_t) 4;

  uint32_t ccr = DMA_CCR_MINC | DMA_CCR_MSIZE_16BIT | DMA_CCR_PSIZE_16BIT;

  ccr |= DMA_CCR_PL_VERY_HIGH | DMA_CCR_DIR | DMA_CCR_CIRC;

  ccr |= DMA_CCR_HTIE | DMA_CCR_TCIE | DMA_CCR_TEIE;

  DMA1_CCR4 = ccr;

As said earlier, I have interrupt at wrong moments of CLK

void dma1_channel4_7_dma2_channel3_5_isr()

{

//  TIM3_SR &= ~TIM_SR_CC1IF;

  static int cnt = 0;

  timDump[cnt++] = TIM3_CNT;

  if(cnt == 50) cnt = 0;

}

timDump = 3817, 3913, 4009, 4105, 4201 ...

stm32f030f4p6 MCU.

This topic has been closed for replies.
Best answer by Tesla DeLorean

BSRR should be 32-bit wide

ARR = N-1 for Divide by N

CNT will be zero at update event, and thus DMA HT/TC IRQs

TIM3_UP is channel 3 on the DMA, not 4

7 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
September 15, 2019

BSRR should be 32-bit wide

ARR = N-1 for Divide by N

CNT will be zero at update event, and thus DMA HT/TC IRQs

TIM3_UP is channel 3 on the DMA, not 4

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MBelk
MBelkAuthor
Associate II
September 15, 2019

Thank you, but I want to clock on compare event, not update

Tesla DeLorean
Guru
September 15, 2019

For Channel 4 (TIM3_CH1), you'd need to configure TIM3->CCR1 and enable it

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User
September 15, 2019

Read out and check/post content of relevant TIM and DMA registers.

JW

MBelk
MBelkAuthor
Associate II
September 16, 2019

checked

waclawek.jan
Super User
September 16, 2019

And did you find the problem?

Do you check and clear the DMA status flag which causes the DMA ISR to be invoked?

JW

MBelk
MBelkAuthor
Associate II
September 16, 2019

checked