Why HAL_UARTEx_ReceiveToIdle_DMA stops working after unpluging serial line and then pluging it back?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-05-05 2:41 PM
I'm experimenting with bluepill, I have set USART3 to DMA circular mode. I've enabled the HAL_UARTEx_ReceiveToIdle_DMA in the main() and then again in the HAL_UARTEx_RxEventCallback, the half complete receive callback is disabled in both main() and in the RxEventCallback. When I start up the bluepill with a serial terminal on windows via uart3, it works fine; but if I unplug the serial line from PC (with the bluepill on) and then plug it back to PC, the uart3 won't receive anything (even though I can see the PC sending bytes on the RX line with a scope). I've placed a breakpoint inside the RxEventCallback, and it won't trigger after uplugging and plugging the serial line back. What's the problem here?
- Labels:
-
DMA
-
UART-USART
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-05-05 5:17 PM
Does this look similar?
https://community.st.com/s/question/0D53W00001XMsHfSAL/stm32f407-usart6-dma-not-receiving-data