cancel
Showing results for 
Search instead for 
Did you mean: 

Why ADC watchdog is not triggering.

SConf
Associate II

The code is as follows....

RCC_AHBPeriphClockCmd (RCC_AHBPeriph_DMA1, ENABLE);

RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC, ENABLE);

RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);

RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO, ENABLE);

static RCC_ClocksTypeDef clocks;

RCC_GetClocksFreq(&clocks);

// Analog inputs - GPIO

GPIO_InitTypeDef GPIO_InitStructure = {0};

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN;

GPIO_Init(GPIOC, &GPIO_InitStructure);

DMA_DeInit(DMA1_Channel1);

DMA_InitTypeDef DMA_InitStructure;

DMA_InitStructure.DMA_PeripheralBaseAddr = ADC1_DR_Address;

DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)&g_analogInput1RawData[0];

DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC;

DMA_InitStructure.DMA_BufferSize = 3;

DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;

DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;

DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;

DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;

DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;

DMA_InitStructure.DMA_Priority = DMA_Priority_High;

DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;

DMA_Init(DMA1_Channel1, &DMA_InitStructure);

DMA_Cmd(DMA1_Channel1, ENABLE);

// TODO for test only DMA_ITConfig(DMA1_Channel1, DMA_IT_TC | DMA_IT_TE, ENABLE);

NVIC_InitTypeDef NVIC_InitStructure;

// ADC Interrupt

NVIC_InitStructure.NVIC_IRQChannel = ADC1_2_IRQn;

NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x00;

NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x00;

NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

NVIC_Init(&NVIC_InitStructure);

// DMA Interrupt

NVIC_InitStructure.NVIC_IRQChannel = DMA1_Channel1_IRQn;

NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

NVIC_Init(&NVIC_InitStructure);

ADC_DeInit(ADC1);

ADC_InitTypeDef ADC_InitStructure;

ADC_InitStructure.ADC_Mode = ADC_Mode_Independent;

ADC_InitStructure.ADC_ScanConvMode = ENABLE;

ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;

ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None;

ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;

ADC_InitStructure.ADC_NbrOfChannel = 3;

ADC_Init(ADC1, &ADC_InitStructure);

ADC_RegularChannelConfig(ADC1, ADC_Channel_10, 1, ADC_SampleTime_55Cycles5);

ADC_RegularChannelConfig(ADC1, ADC_Channel_11, 2, ADC_SampleTime_55Cycles5);

ADC_RegularChannelConfig(ADC1, ADC_Channel_12, 3, ADC_SampleTime_55Cycles5);

ADC_Cmd(ADC1, ENABLE);

ADC_DMACmd(ADC1, ENABLE);

ADC_ITConfig(ADC1, ADC_IT_AWD , ENABLE);

ADC_ResetCalibration(ADC1);

while (ADC_GetResetCalibrationStatus(ADC1));

ADC_StartCalibration(ADC1);

while (ADC_GetCalibrationStatus(ADC1));

uint16_t lowThreshold = 3700;

uint16_t highThreshold = 3500;

ADC_AnalogWatchdogThresholdsConfig(ADC1, highThreshold, lowThreshold);

ADC_AnalogWatchdogCmd(ADC1, ADC_AnalogWatchdog_SingleRegEnable);

ADC_AnalogWatchdogSingleChannelConfig(ADC1, ADC_Channel_0);

ADC_SoftwareStartConvCmd(ADC1, ENABLE);

The registers seem to be set correctly....

0690X000006CFSmQAO.jpg

The analog voltage read in is 3794. Since the high threshold is 3700 shouldn't the analog watchdog have been triggered?

1 REPLY 1
SConf
Associate II

​Correction...

uint16_t lowThreshold = 3300;

uint16_t highThreshold = 3500;

Actual still 3794.

I was changing thresholds to and the previous was incorrect. No matter what the threshold I don't get the interrupt.