2022-08-08 1:28 AM
Currently I am trying to use ibis model for simulation. I found ibis model file provided by STMicro and try to use them. But I could not figure out which model pointed by model selector I should use.
For example, there are 24 candidates of the model for PA0. But I don't know which one for my project.
Actual .ibs files is like below.
Thanks.
[Pin] signal_name model_name R_pin L_pin C_pin
...
6 PA0 io8p_wsudq_ls_ft_v33 61.160E-3 1.8629E-9 10.243E-15
...
[Model Selector] io8p_wsudq_ls_ft_v33
io8p00_wsudq_ls_ft_v33_pd_lv "SPEED00 1P8V, PD=40kOhm"
io8p00_wsudq_ls_ft_v33_pu_lv "SPEED00 1P8V, PU=40kOhm"
io8p00_wsudq_ls_ft_v33_lv "SPEED00 1P8V"
io8p01_wsudq_ls_ft_v33_pd_lv "SPEED01 1P8V, PD=40kOhm"
io8p01_wsudq_ls_ft_v33_pu_lv "SPEED01 1P8V, PU=40kOhm"
io8p01_wsudq_ls_ft_v33_lv "SPEED01 1P8V"
io8p10_wsudq_ls_ft_v33_pd_lv "SPEED10 1P8V, PD=40kOhm"
io8p10_wsudq_ls_ft_v33_pu_lv "SPEED10 1P8V, PU=40kOhm"
io8p10_wsudq_ls_ft_v33_lv "SPEED10 1P8V"
io8p11_wsudq_ls_ft_v33_pd_lv "SPEED11 1P8V, PD=40kOhm"
io8p11_wsudq_ls_ft_v33_pu_lv "SPEED11 1P8V, PU=40kOhm"
io8p11_wsudq_ls_ft_v33_lv "SPEED11 1P8V"
io8p00_wsudq_ls_ft_v33_pd "SPEED00, PD=40kOhm"
io8p00_wsudq_ls_ft_v33_pu "SPEED00, PU=40kOhm"
io8p00_wsudq_ls_ft_v33 "SPEED00"
io8p01_wsudq_ls_ft_v33_pd "SPEED01, PD=40kOhm"
io8p01_wsudq_ls_ft_v33_pu "SPEED01, PU=40kOhm"
io8p01_wsudq_ls_ft_v33 "SPEED01"
io8p10_wsudq_ls_ft_v33_pd "SPEED10, PD=40kOhm"
io8p10_wsudq_ls_ft_v33_pu "SPEED10, PU=40kOhm"
io8p10_wsudq_ls_ft_v33 "SPEED10"
io8p11_wsudq_ls_ft_v33_pd "SPEED11, PD=40kOhm"
io8p11_wsudq_ls_ft_v33_pu "SPEED11, PU=40kOhm"
io8p11_wsudq_ls_ft_v33 "SPEED11"
Solved! Go to Solution.
2022-08-10 8:52 AM
Hello,
Actually the choice of the needed submodel depends on your use case. Below you can find some clarifications about the models:
IO speed: speed00: low speed, speed01: medium, speed10: high, speed11: very high
pd: pull down, pu: pull up
Best regards,
2022-08-10 8:52 AM
Hello,
Actually the choice of the needed submodel depends on your use case. Below you can find some clarifications about the models:
IO speed: speed00: low speed, speed01: medium, speed10: high, speed11: very high
pd: pull down, pu: pull up
Best regards,
2022-08-21 5:29 PM
Thank you for your help. You helped me a lot and solve what I could not understand. I thought the electricity property should depend on actual setting on MCU and I didn't know what "SPEED" or "PD" mean.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.