cancel
Showing results for 
Search instead for 
Did you mean: 

Where should I report a correction to the F37x Clock Configuration Tool?

gfuehrer
Associate II
Posted on April 11, 2013 at 20:30

Does anyone know where to report mistakes in STmicro downloads, whether its tools, datasheets, or firmware libraries? I have others to report.

The line in SystemInit to reset CFGR3 is wrong. It should read:

  RCC->CFGR3 &= (uint32_t)0xFFF0F

F

8C;

#stmf37x-clock-configuration-bug
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
gfuehrer
Associate II
Posted on April 19, 2013 at 18:17

*ping* Anyone? I keep finding more mistakes in docs and firmware that I'd like to report and move on.

Thanks,

-Gary

[Soapbox] Another reason to use a normal source code system like github or code.google -- bug reporting is an obvious and natural feature that is already built-in.

Posted on April 19, 2013 at 18:32

The error is also in the code for the firmware library.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Amel NASRI
ST Employee
Posted on May 09, 2013 at 16:35

Hello Gary,

Thanks for reporting, it is noted.

What other ''bugs/errors'' do you want to highlights? You can do it here.

Best Regards,

ST.MCU

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.