cancel
Showing results for 
Search instead for 
Did you mean: 

Where is the MCU's ID?

Workalot
Associate III
Posted on July 18, 2017 at 13:51

Workalot would like to obtain the MCU's ID, just like the STM32 ST-Link utility does. It reports an ID 0x413 and a 1MB Flash for my STM32F4Discovery.

To be clear, I am not after the 96 bit UID (at 0x1FFF7A10) nor am I looking for the SCB.CPUID (ARM CPU).

Such details surely reside in the MCU's ROM memory space. I look at documentation but I must looking in the wrong places.

thank you and regards,

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
john doe
Lead
Posted on July 18, 2017 at 14:02

It's in the DBGMCU_IDCODE register. check the reference manual for your chip.

    uint8_t len = 0;

    char devidString[128] = {0};

    uint32_t idcode = DBGMCU->IDCODE & 0xFFF;

    switch (idcode)

    {

    case 0x410: len += sprintf(devidString+len, 'stm32f1xx medium-density'); break;

    case 0x411: len += sprintf(devidString+len, 'stm32f2xx'); break;

    case 0x412: len += sprintf(devidString+len, 'stm32f1xx low-density'); break;

    case 0x413: len += sprintf(devidString+len, 'stm32f405/407xx and stm32f415/417xx'); break;

    case 0x414: len += sprintf(devidString+len, 'stm32f1xx high-density'); break;

    case 0x415: len += sprintf(devidString+len, 'stm32l4xx'); break;

    case 0x416: len += sprintf(devidString+len, 'stm32l1xx medium-density'); break;

    case 0x417: len += sprintf(devidString+len, 'stm32l0xx'); break;

    case 0x418: len += sprintf(devidString+len, 'stm32f1xx connectivity line'); break;

    case 0x419: len += sprintf(devidString+len, 'stm32f4xx high-density'); break;

    case 0x420: len += sprintf(devidString+len, 'stm32f1xx value line'); break;

    case 0x421: len += sprintf(devidString+len, 'stm32f446xx'); break;

    case 0x422: len += sprintf(devidString+len, 'stm32f3xx'); break;

    case 0x423: len += sprintf(devidString+len, 'stm32f4xx low power'); break;

    case 0x425: len += sprintf(devidString+len, 'stm32l0xx cat. 2'); break;

    case 0x427: len += sprintf(devidString+len, 'stm32l1xx medium-density/plus'); break;

    case 0x428: len += sprintf(devidString+len, 'stm32f1xx value line high-density'); break;

    case 0x429: len += sprintf(devidString+len, 'stm32l1xx cat. 2'); break;

    case 0x430: len += sprintf(devidString+len, 'stm32f1xx xl-density'); break;

    case 0x431: len += sprintf(devidString+len, 'stm32f411re'); break;

    case 0x432: len += sprintf(devidString+len, 'stm32f37x'); break;

    case 0x433: len += sprintf(devidString+len, 'stm32f4xx de'); break;

    case 0x434: len += sprintf(devidString+len, 'stm32f4xx dsi'); break;

    case 0x435: len += sprintf(devidString+len, 'stm32l43x'); break;

    case 0x436: len += sprintf(devidString+len, 'stm32l1xx high-density'); break;

    case 0x437: len += sprintf(devidString+len, 'stm32l152re'); break;

    case 0x438: len += sprintf(devidString+len, 'stm32f334'); break;

    case 0x439: len += sprintf(devidString+len, 'stm32f3xx small'); break;

    case 0x440: len += sprintf(devidString+len, 'stm32f0xx'); break;

    case 0x441: len += sprintf(devidString+len, 'stm32f412'); break;

    case 0x442: len += sprintf(devidString+len, 'stm32f09x'); break;

    case 0x444: len += sprintf(devidString+len, 'stm32f0xx small'); break;

    case 0x445: len += sprintf(devidString+len, 'stm32f04x'); break;

    case 0x446: len += sprintf(devidString+len, 'stm32f303 high-density'); break;

    case 0x447: len += sprintf(devidString+len, 'stm32l0xx cat. 5'); break;

    case 0x448: len += sprintf(devidString+len, 'stm32f0xx can'); break;

    case 0x449: len += sprintf(devidString+len, 'stm32f74xxx/stm32f75xxx'); break;

    case 0x450: len += sprintf(devidString+len, 'stm32h7xxx'); break;

    case 0x451: len += sprintf(devidString+len, 'stm32f76xxx/stm32f77xxx'); break;

    case 0x452: len += sprintf(devidString+len, 'stm32f72xxx/stm32f73xxx'); break;

    case 0x457: len += sprintf(devidString+len, 'stm32l011'); break;

    case 0x458: len += sprintf(devidString+len, 'stm32f410'); break;

    case 0x463: len += sprintf(devidString+len, 'stm32f413'); break;

    default: len += sprintf(devidString+len, 'unknown device\r\n');

    }

    uint32_t revCode = (DBGMCU->IDCODE & DBGMCU_IDCODE_REV_ID_Msk) >> DBGMCU_IDCODE_REV_ID_Pos;

    switch (revCode)

    {

    case 0x1000: len += sprintf(devidString+len, '  Revision A\r\n'); break;

    case 0x1001: len += sprintf(devidString+len, '  Revision Z\r\n'); break;

    }

/*

          For example, it is read as RevA -> 0x1000, Cat 2 revZ -> 0x1001, rev1 -> 0x1003, rev2 ->0x1007, revY -> 0x100F for STM32F405/407xx and STM32F415/417xx devices

          For example, it is read as RevA -> 0x1000, Cat 2 revY -> 0x1003, rev1 -> 0x1007, rev3 ->0x2001 for STM32F42xxx and STM32F43xxx devices

          For example, it is read as RevZ -> 0x1000, Cat 2 revA -> 0x1001 for STM32F401xB/C devices

          For example, it is read as RevA -> 0x1000, Cat 2 revZ -> 0x1001 for STM32F401xD/E devices

          For example, it is read as RevA -> 0x1000 for STM32F411xx,STM32F413/423xx,STM32F469/423xx, STM32F446xx and STM32F410xx devices

          For example, it is read as RevZ -> 0x1001, Cat 2 revB -> 0x2000, revC -> 0x3000 for STM32F412xx devices

*/

    printf('%s', devidString);

Imen.D
ST Employee
Posted on July 18, 2017 at 14:05

Hello,

Look at your reference manual RM0090 in ( 38.6.1 MCU device ID code )

Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on July 18, 2017 at 15:14

DBGMCU_IDCODE

0xE0042000

Use it here in system_stm32f4xx.c to detect the specific part and set clocks/plls optimally.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Workalot
Associate III
Posted on July 18, 2017 at 22:47

Yes, I knew it had to be a simple thing. Thank you all for your promptness and accuracy.

Regards, Workaot

john doe
Lead
Posted on July 19, 2017 at 01:39

>It reports an ID 0x413 and a 1MB Flash for my STM32F4Discovery.

You can determine the flash size by reading FLASHSIZE_BASE register which is defined in STM32Cube_FW_F4_V1.16.0/Drivers/CMSIS/Device/ST/STM32F4xx/Include/stm32f407xx.h