cancel
Showing results for 
Search instead for 
Did you mean: 

where i can find an example for dual CDC VCP on stm32?

mirko2399
Associate II
Posted on August 17, 2016 at 00:56

I should use the USB FS on CN5 of STM32F4-Discovery in dual Virtual Com Port (if possible in three VCP).

I made a project started from cubemx with USB_CDC_VCP with USBD_MAX_NUM_INTERFACES = 3 and USBD_MAX_NUM_CONFIGURATION=3 .

It work well but in the pc instal one COM only.

I tryed to modify the usb descriptor manually but it not work fine. I have Always one COM only.

Where i can find un example based on cubemx library whith multiple CDC VCP?

Very Thank.
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Amel NASRI
ST Employee
Posted on August 17, 2016 at 11:35

Hi lor3n7o,

USB composite isn't supported yet by CubeMX.

I report your request internally for farther review. We will keep you informed if we have more details on this regard.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

mirko2399
Associate II
Posted on August 17, 2016 at 11:58

Very thanks for faster support.

mirko2399
Associate II
Posted on August 19, 2016 at 10:01

There is un example not based on cubemx library with multiple CDC VCP on USBFS on stm32f4,on which I can relate for implementation in may project?

In the meantime I might try to do a manual edit.

Very Thank.