2014-07-21 07:07 AM
Hello,
I'm using the STM32F205RG chip (WLCSP64 package) This chip has no dedicated pins for VDDA/GNDA. Are these connections shared with a specific VDD/GND pin? If so which one? The goal of my question is to make a nice ground separation for analog and digital and improve ADCs/DACs performance. Cheers, Simon2014-07-21 07:22 AM
But it does have dedicated Vcap1 & Vcap2 pins. See Figure 19 in the data sheet.
Cheers, Hal