cancel
Showing results for 
Search instead for 
Did you mean: 

What is the proper method to re-initialize SD card interface to support removal/reinsertion of SD card?

Tim Russell
Associate III

My SD card interface (using SDMMC1) stops working after the SD card has been removed/re-inserted.

I have tried un-mounting using f_mount(0, &SDPath, 0) and then re-mounting with no success.

As a test, I executed the following for each transaction:

f_mount(&SDFatFs, &SDPath, 0);

f_open(&SDFile,.....);

f_write(&SDFile, .....);

f_close(&SDFile);

f_mount(0, &SDPath, 0);

If I remove/re-insert the SD card after the 1st transaction, I get an FR_DISK_ERR error on the f_open() on the second transaction (following the reinsertion of the SD card). I have traced this error down into the HAL_SD_ReadBlocks_DMA() functions which gets a timeout on the call to SDMMC_CmdBlockLength(hsd->Instance, BLOCKSIZE).

Any suggestions?

This discussion is locked. Please start a new topic to ask your question.
20 REPLIES 20

thank you so much <3